Application Common Services
Digital App Center
The dashboards and the application build are deployed using the Digital Apps Center (DAC). Following are the features in
Genix Suite 25.2
Flexible Navigation using Breadcrumb
Breadcrumb have configurable links and dropdowns that allows navigation with pages that use the same source page. For example, if same configuration page is reused by multiple application, the link in the breadcrumb can be configured to redirect to the same configuration page.